Compressibility Calculation Error Code

Associated with: Flow runs

This attribute indicates whether the Flow Run’s Compressibility Calculation has generated an error. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller. Information is displayed in this format:

<Error Code>:<Description>

where 0: No error indicates that the calculation has recalculated successfully. If an error has occurred, a 5-digit error code and corresponding description is displayed.

Example:

20002: Inputs have not been configured

For a list of compressibility calculation error codes and their corresponding descriptions, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2022