Contract Properties

The fields within the Contract section of the Flow Run tab display those configuration properties that are associated with the output of the flow calculation.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

The settings on the Contract section allows you to define the parameters for the gas, liquid, or water measurement contract. This is referred to as contract configuration because these parameters are often defined by a contract for selling gas, liquid, or water.

Further Information

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2022