Gas Flow Application Build Number

Associated with: Realflo controllers

This attribute indicates the build number of the Gas Flow application that is running on the controller. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.

Example:

5


Disclaimer

Geo SCADA Expert 2022