Inputs Properties

The Inputs section of the Flow Run tab is common to all of the flow run types. You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

Use the following fields within the Inputs section of the Flow Run tab to define the properties that are associated with the flow calculation’s input values:

The properties that you configure in the Inputs section are used for the water cut, differential pressure, static pressure, density, temperature inputs, or the pulse input frequency, as applicable to the type of Flow Run and calculation that is being performed.

Further Information

Measurement Units.

For more detailed information on these properties, see the documentation provided with the Realflo application.


Disclaimer

Geo SCADA Expert 2022