Source (Gas Flow Run)
Associated with: SCADAPack Modbus Realflo Outsations, and SCADAPack Modbus Realflo Analog Input points
The Source attribute is common to many Status displays. The attribute indicates the location at which an item resides. The information shown varies, depending on the type of item.
For SCADAPack Modbus Realflo Outstations, the attribute displays information in this format:
Set <Set Address>:OS <Controller Address>
For SCADAPack Modbus Realflo Analog Inputs, the attribute displays information in this format:
Set <Set Address>:OS <Controller Address>:Flow Run <Flow Run Number>:AI Source <Source Number>:Item <Item Number> (Address <Point Address>)
where:
- <Source Number> represents the type of Flow Run Source defined for the Analog Input Point
- <Item Number> represents the type of Flow Run Data Item defined for the Analog Input Point.
For information about either of the above properties, see Configure the General Realflo Analog Point Properties.
The table below indicates the type of Flow Run Source <Source Number > represents.
| Source Number | Source Type |
|---|---|
| 0 | Accumulation |
| 1 | Input |
| 2 | Flow Calculation |
| 3 | Compressibility Calculation |
| 4 | Density Calculation |
| 10 | Daily Flow History |
| 11 | Hourly History Data |
| 12 | Batch Records |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Accumulation (<Source Number>=0).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Uncorrected flow volume during previous month (AGA-7 and AGA-9 only) |
| 2 | Uncorrected flow volume during current month (AGA-7 and AGA-9 only) |
| 3 | Uncorrected flow volume during previous contract day (AGA-7 and AGA-9 only) |
| 4 | Uncorrected flow volume during current contract day (AGA-7 and AGA-9 only) |
| 5 | Number of flow calculations during contract day |
| 6 | Duration of flow during contract day |
| 7 | Flow volume at base conditions during contract day (gas only) |
| 8 | Flow mass at base conditions during contract day (gas only) |
| 9 | Flow energy at base conditions during contract day (gas only) |
| 10 | Total accumulated flow volume at base conditions (gas only) |
| 11 | Flow duration in current month |
| 12 | Flow volume in current month |
| 13 | Flow duration in previous month |
| 14 | Flow volume in previous month |
| 15 | Duration of flow during previous contract day |
| 16 | Flow volume at base conditions during previous contract day |
| 17 | Flow mass at base conditions during previous contract day |
| 18 | Flow energy at base conditions during the previous contract day |
| 19 | Number of flow calculations during previous contract day |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Input (<Source Number>=1).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Calibration flags |
| 2 | Temperature Input Alarm |
| 3 | Static Pressure Input Alarm |
| 4 | Differential Pressure Input Alarm (AGA-3 and V-Cone only) |
| 4 | Turbine Pulse Rate Input Alarm (AGA-7 only) |
| 4 | USM Pulse Rate Input Alarm (AGA-9 only) |
| 4 | Mass Flow Input Alarm (AGA-11/Liquid/Water) |
| 4 | Mass Pulse Input Alarm (AGA-11/Liquid/Water) |
| 5 | Live Turbine Meter Pulse Rate (AGA-7 only) |
| 5 | Live USM Pulse Rate (AGA-9 only) |
| 5 | Live Mass Pulse Rate (AGA-11/Liquid/Water Mass Pulse) |
| 6 | Live Temperature |
| 7 | Live Static Pressure |
| 8 | Live Differential pressure (AGA-3 and V-Cone only) |
| 8 | Live Mass Flow (AGA-11/Liquid/Water) |
| 9 | Forced Temperature |
| 10 | Forced Static Pressure |
| 11 | Forced Differential Pressure (AGA-3 and V-Cone only) |
| 11 | Forced Mass Flow (AGA-11/Liquid/Water) |
| 12 | Forced Turbine Pulse Rate (AGA-7 only) |
| 12 | Forced USM Pulse Rate (AGA-9 only) |
| 12 | Forced Mass Pulse Rate (AGA-11/Liquid/Water Mass Pulse) |
| 13 | Current Turbine Meter Pulse Rate (AGA-7 only) |
| 13 | Current USM Pulse Rate (AGA-9 only) |
| 13 | Current Mass Pulse Rate (AGA-11/Liquid/Water Mass Pulse) |
| 14 | Current Differential Pressure (AGA-3 and V-Cone only) |
| 14 | Current Mass Flow (AGA-11/Liquid/Water) |
| 17 | Current Input Temperature |
| 18 | Current Static Pressure |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Flow Calculation (<Source Number>=2).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Compressibility approximated flag |
| 2 | Input or flow calculation error code |
| 3 | Flow volume rate |
| 4 | Flow mass rate |
| 5 | Flow energy rate (gas only) |
| 6 | Flow extension (AGA-3 1992/2013 only) |
| 6 | Flow product (AGA-3 1985 only) |
| 6 | Uncorrected flow volume (AGA-7 and AGA-9 only) |
| 7 | Date of Flow Update |
| 8 | Time of Flow Update |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Compressibility Calculation (<Source Number>=3).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Compressibility calculation result code |
| 2 | Supercompressibility |
| 3 | Real relative gas density |
| 4 | Mass density at flow conditions |
| 5 | Mass density at base conditions |
| 6 | Date of Compressibility Update |
| 7 | Time of Compressibility Update |
| 8 | Calculated Speed of Sound (available from Realflo 7.02.1 onwards) |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Density Calculation (<Source Number>=4).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Heating value |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Daily Flow History (<Source Number>=10), or Hourly History Data (<Source Number>=11).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Duration of flow in period |
| 2 | Flow volume at base conditions |
| 3 | Flow mass at base conditions |
| 4 | Flow energy at base conditions |
| 5 | Flow extension (AGA-3 1992/2013 only) |
| 5 | Flow product (AGA-3 1985 only) |
| 5 | Uncorrected flow volume (AGA-7 and AGA-9 only) |
| 5 | Integral value (AGA-11 Only) |
| 6 | Average temperature |
| 7 | Average static pressure |
| 8 | Average differential pressure (AGA-3 and V-Cone only) |
| 8 | Average Mass Flow (AGA-11 Mass Flow Only) |
| 9 | Average number of rotations per second (AGA-7 and AGA-11 Mass Pulse only) |
| 10 | Average real relative gas density |
| 11 | Input Units |
| 12 | Contract Units |
| 13 | Number of Alarms |
| 14 | Number of Events |
| 26 | Batch ID |
| 27 | Duration of period |
| 28 | QTR Identifier |
The table below indicates the type of Flow Run Data Item <Item Number > represents, when the Source Type for the Analog Input Point is defined as Batch Records (<Source Number>=12).
| Item Number | Gas Flow Run Data Item Type |
|---|---|
| 1 | Flow Time |
| 2 | Flow volume at base conditions |
| 3 | Flow mass at base conditions |
| 4 | Flow energy at base conditions |
| 5 | Uncorrected flow volume (AGA-7 and AGA-9 only) |
| 5 | Flow extension (AGA-3 1992/2013 only) |
| 5 | Flow product (AGA-3 1985 only) |
| 5 | Integral Value (AGA-11 Only) |
| 6 | Average Temperature |
| 7 | Average Pressure |
| 8 | Average differential pressure (AGA-3 and V-Cone only) |
| 8 | Average Mass Flow (AGA-11 Mass Flow Only) |
| 9 | Average number of rotations per second (AGA-7 and AGA-11 Mass Pulse only) |
| 10 | Average real relative gas density |
| 11 | Input Units |
| 12 | Contract Units |
| 13 | Alarm Count |
| 14 | Event Count |
| 26 | Batch ID |
| 27 | Duration of period |
| 28 | QTR Identifier |