User Number

Associated with: Realflo controllers

This attribute displays the User Number that is associated with the controller’s User ID name. (The User ID is defined on the Realflo tab of the controller’s configuration Form—see Specify the User ID and Passcode that Allow Access to the Realflo Components.) The attribute is displayed once a controller is or has been in communication with the server.

Example:

1


Disclaimer

Geo SCADA Expert 2022