Configure the USB Communications
The USB Communications section of the Settings tab allows you to enable USB communications with the outstation if required.
Select the Enabled box if USB communications is a required feature.