SCADAPack x70

Defining Identification Strings

The Settings tab on the Forms of SCADAPack x70 Device Configuration items includes an Identification Strings section. Use the section to specify Identification information about an outstation.

You can specify the following:

Location Name

Enter the name or code of the location where the outstation is installed. You can enter text in any format. Maximum 255 characters including spaces. For example, '1267 Main Street', 'Highfield Reservoir' or 'SO 12300 45678'.

ID Code/Number

Enter the code or number that is assigned to the device. You can enter text in any format. Maximum 32 characters including spaces. For example, '1234' or '99-ZZ'.

Device Name

Enter the name that is assigned to the device. You can enter text in any format. Maximum 32 characters including spaces. For example, '12345RTU678' or 'High Street Sub'.


Disclaimer

Geo SCADA Expert 2022