Number of Modbus Server Devices
Associated with: SCADAPack x70 Device Configuration items.
The Number of Modbus Server Devices status attribute indicates the number of SCADAPack x70 Modbus Server Device items that are associated with the selected SCADAPack x70 Device Configuration item. You use this status attribute to determine the number of Modbus Server Device items that are currently associated with, and/or can still be associated with, the SCADAPack x70 Device Configuration item within the given limit. You can add a maximum of 150 Modbus Server Device items to a SCADAPack x70 device. If there are no associated Modbus Server Device items, the status attribute displays the value '0'.
For information about Modbus Server Devices, see Configure a Modbus Server Device.