Specify the Point's Modbus Register Address
The Modbus tab on the Forms of SCADAPack x70 Analog, Digital, and Counter Configuration items contains a Modbus Register field.
Use the field to specify the Modbus register to which the point's values are to be mapped in the SCADAPack x70 device.
The valid Modbus register addresses are:
Value Type | Address Range | Description |
---|---|---|
Input values | 30001-39999 | Read-only input registers |
Output values | 40001-49999 | Read/write holding registers |