SCADAPack x70

Specify the Required Input Filter

An Input Filter field is displayed on the SCADAPack x70 tab of I/O Modules that support this option. Use the filter to dampen measurement variation or noise on analog inputs, or reduce noise on digital inputs. The options that are available vary, depending on the type of point to which the filter relates. In each case, the setting is applied to all inputs of that type on the I/O Module.

The Input Filter for analog inputs typically provides these options:

 

The Input Filter for RTD analog inputs can be used to dampen process variations or noise. The input filter provides these options:

 

The Input Filter for digital inputs provides these options:


Disclaimer

Geo SCADA Expert 2022