Force Poll for Current Dynacard
Associated with: SE Rod Pump Controllers
Security permission required to access this pick action: Retrieve Data
Geo SCADA Expert can retrieve an SE Rod Pump controller's current dynacard data automatically, at the frequency specified on the Outstation Form (see Define the Dynacard Poll Intervals).
If required, use the Force Poll for Current Dynacard pick action to retrieve new current dynacard data between scheduled polls. When executed, the pick action triggers Geo SCADA Expert to poll (scan) the controller for current dynacard data. Should Geo SCADA Expert detect that the controller has current data for a new stroke, it will retrieve the data for that new stroke.
NOTE: If using this pick action with the Automation Interface, you have to specify the method name UploadCurrentDynacard.