Minimum Configuration

This topic relates to controllers on the SE Rod Pump Controller driver.

When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:

 

For a controller on this driver to be capable of functioning in Geo SCADA Expert, as a minimum you have to specify these properties on the item's configuration Form:

 

Also ensure that the controller and the database items on which it depends are In Service, and have saved, valid configuration. This will produce a controller that is capable of functioning using the default configuration settings.


Disclaimer

Geo SCADA Expert 2022