Upload Historic Data
Associated with: SE Rod Pump controllers
Security permission required to access this pick action: Retrieve Data
Geo SCADA Expert can upload an SE Rod Pump controller’s historic point data automatically, at the frequency specified on the Outstation Form (see Define the Historic Data Poll Interval).
If required, you can also use the Upload Historic Data pick action to upload the point data that is stored in the controller's historic buffers.
NOTE: If using this pick action with the Automation Interface, you have to specify the method name UploadHistoric.