ASN Data Type

Associated with: SNMP points

The syntax used for SNMP is Abstract Syntax Notation 1 (ASN.1). The syntax defines, for example, the type of data that is accessed using the SNMP protocol. ASN.1 is used within the MIB database at each SNMP database.

The ASN Data Type attribute indicates the data type with which the point is associated.

Possible States: These vary, depending on the point type:

Every type of point:

SNMP Integer, Cardinal, and Digital points support these data types:

Additionally, SNMP Integer points support these data types:

SNMP String points support these data types:

Geo SCADA Expert does not support the data types ASN OBJECT IDENTIFIER or ASN COUNTER64.


Disclaimer

Geo SCADA Expert 2022