Configure the Trap Specific Properties

If the point is used to retrieve technology-, product- or user-specific trap information (as opposed to Poll or Generic trap data), you need to specify the trap-specific details in the Trap Specific section of the <Point Type> tab. These properties define the trap-specific information that is to appear in any data packets sent by the SNMP agent, to identify which alarm or event the agent is reporting.

The fields within the Trap Specific section of the <Point Type> tab are only available for use when the point Action is set to Trap Specific (see Configure the Common Point Properties).

The SNMP driver allows you to keep the same configuration as SNMP v1. The SNMP driver translates SNMPv2 notification parameters to SNMPv1 notification parameters


Disclaimer

Geo SCADA Expert 2022