Export SQL Query Result
Associated with: SQL Exports
Security permission required to access this pick action: Control
If the data is being exported to removable media, please check that the media is at the required location and is available for use. For example, if the data is to be stored on a CD-R, a suitable CD-R needs to be inserted in the CD-RW driver of the server before the SQL query result is exported.
Use this pick action to execute the SQL Query that is associated with an SQL Export item and export the result of that query. The location to which Geo SCADA Expert exports the result and the format that the output file takes is pre-defined, using fields on the SQL Export Form (see Add and Configure an SQL Export).
If the result of the SQL Query is being exported to a file that is accessed via a UNC path, Geo SCADA Expert uses a Windows® user account to export the created file and create any subfolders. The particular Windows user account that is used for exporting the results of SQL Queries is that specified for the Printer User (see Printer Settings). This Windows user account has to have permission to create files and folders in the specified share on the specified file server.
If you are using this pick action with the Automation Interface, you need to specify the method name Export. (Refer to the Database Schema for argument naming conventions used with the Automation Interface.)