Expressions.expr-primary-location
A Location string, used to define a location using latitude and longitude within a query.
LOCATION <Location string>
Format
LOCATION { 'Location string' | ? | ( LocationExpr ) }
The Location string format is defined as follows:
Latitude, Longitude [, Accuracy] [ALT Altitude [, Altitude-Accuracy]] [DIR Heading, Speed] [TS yyyy-MM-dd [HH:mm:ss.SSS]]
where components (see Accuracy and Altitude) in [ ] are optional.
The following are examples of the how the components maybe combined within the Location string:
Latitude, Longitude
Latitude, Longitude [, Accuracy]
Latitude, Longitude [ALT Altitude]
Latitude, Longitude [ALT Altitude [, Altitude Accuracy]]
Latitude, Longitude [DIR Heading, Speed]
Latitude, Longitude [TS yyyy-MM-dd]
Latitude, Longitude [TS yyyy-MM-dd [HH:mm:ss.SSS]]
Latitude, Longitude [, Accuracy] [ALT Altitude [, Altitude Accuracy]] [DIR Heading, Speed] [TS yyyy-MM-dd [HH:mm:ss.SSS]]
The following table describes the required format for each component:
| Type | Format |
|---|---|
| Latitude, Longitude |
Degrees as a decimal number, for example: 10.14563, 51.2368. |
| Accuracy (for Latitude & Longitude) | Meters, (this data is normally provided by GPS systems), this allows you to refine a location query by the accuracy of the Latitude and Longitude data. |
| ALT Altitude | Meters, above mean sea level. |
| Altitude-Accuracy | Meters, allows you to define the accuracy of altitude position. |
| DIR Heading | Heading in degrees clockwise from North. |
| Speed | Meters per second, defines the speed along the heading |
| TS Timestamp | yyyy-MM-dd [HH:mm:ss.SSS] |
All numeric location / region components in location strings use the English decimal point (a dot).
Remarks
Location values are defined using the LOCATION keyword followed by a Location value.
The Location value can be one of the following:
- A string literal containing the standard location format
- A parameter marker.
- A string expression enclosed in parentheses that evaluates to a string containing the standard location format.
Comparison operators IN, NULLIF and CAST functions can be used with LOCATION literals and location database fields.
CAST supports LOCATION AS STRING and STRING AS LOCATION (string containing the standard location format).
Comparison operators can compare LOCATION with LOCATION, LOCATION with STRING and vice versa.
The following example illustrates the use of the LOCATION literal to list the distance (in kilometers) between a set of objects and a specified location. Only objects whose GEOPOSITION is less than Latitude 51 and Longitude 0 are included.
SELECT
NAME, GISLOCATION->GEOPOSITION, DISTANCE( LOCATION '51.476852,0' TO GISLOCATION->GEOPOSITION ) / 1000.0 AS "Distance In Km"
FROM
CDBOBJECT
WHERE
GISLOCATION->GEOPOSITION IS NOT NULL AND GISLOCATION->GEOPOSITION < '51,0'
This produces a list similar to that shown below:
| Row | Name | GISLOCATION->GEOPOSITION | Distance In Km |
|---|---|---|---|
| 0 | Direct Outstation Set | 25, 0 | 2944.0916159 |
| 1 | Analog Input Point 03 | 35, 0 | 1832.1423494 |
| 2 | Analog Input Point 01 | 30, 0 | 2388.1169826 |
| 3 | Analog Input Point 02 | 32, 0 | 2165.7271294 |
Also see: