AlarmBanner.SelectedAlarms
The AlarmBanner.SelectedAlarms property represents a collection of the alarms that are currently selected in the Alarm Banner. It is only available for the Alarm Banner object and so only applies to Alarm Banner scripts.
Syntax |
AlarmBanner.SelectedAlarms |
Description |
Represents the alarms that are currently selected in the Alarm Banner in ViewX. |
Arguments |
None. |
Returns |
Alarm Collection. |
Example:
In this example, the function AllAlarms calls the ReassignAlarm function for the currently selected alarms in the Alarm Banner. The ReassignAlarm function would be defined elsewhere in the script and would define the user to which the alarms are to be reassigned.
Function AllAlarms
for each A in AlarmBanner.SelectedAlarms
ReassignAlarm A
Next
End Function
The letter A
represents each alarm in the collection. A
is simply a variable and you can use any letter or word to represent each alarm.