ComboBox.Count

The ComboBox Control Object that is returned by the AddComboBox function has a Count property. The Count property returns a number that corresponds to the number of options in the Combo Box list.

Syntax

ControlObject.Count

Where ControlObject. is the name of the variable (declared in your script) that is used to store the Combo Box Control Object that is returned by the AddComboBox function.

Description

Returns a numeric value that matches the total number of options in the Combo Box's list. The Count property is read only.

Arguments

None.

Returns

Integer (the total number of options in the Combo Box's list).

Example:

A Combo Box has 6 options. In the script, the following script is used to display a message box containing a count of the options:

MsgBox ComboBox1.Count

Where:

  • ComboBox1 is the name of the variable that is used to store the ComboBox Control Object that is returned by the AddComboBox function. When the script is executed, a message box is displayed containing the number 6 (the total number of options in the Combo Box's list).

Disclaimer

Geo SCADA Expert 2022