EditBox.SetRange

The EditBox.SetRange function allows the script to set an Edit Box to only allow numerical entries within a defined range.

Syntax

ControlObject.SetRange(Min,Max)

Where ControlObject is the name of the variable (declared in your script) that is used to store the EditBox Control Object that is returned by the AddEditBox function.

Description

Sets the Edit Box to only allow numerical entries within a defined range. A spin-box is added to the Edit Box to allow users to scroll through the available settings.

Arguments

Min {integer}

Defines the lowest number permitted in the Edit Box.

 

Max {integer}

Defines the highest number permitted in the Edit Box.

Returns

Integer.

Example:

EditBox1.SetRange 3,50

Where:

  • EditBox1 is the name of the variable that stores the EditBox Control Object returned by the AddEditBox function
  • 3 is the lowest permitted entry
  • 50 is the highest permitted entry.

Disclaimer

Geo SCADA Expert 2022