GroupBox.Height

The GroupBox Control Object that is returned by the AddGroupBox function has a Height property. The Height property represents the height setting of the Group Box.

Syntax

Object.Height = Value

Where Object is the name of the variable (declared in your script) that is used to store the GroupBox Control Object that is returned by the AddGroupBox function.

Description

Sets the height of the Group Box.

Arguments

Value {integer}

Defines the height setting of the Group Box.

Returns

Integer

Example:

GroupBox1.Height = 10

Where:

  • GroupBox1 is the name of the variable that stores the GroupBox Control Object returned by the AddGroupBox function
  • 10 is the height setting for the Group Box.

Disclaimer

Geo SCADA Expert 2022