Mimic.BackColour

The Mimic.BackColour property can be used to set the background color of the Mimic that contains the script.

Syntax

Mimic.BackColour = Color Value

Description

Sets the background color of the Mimic on which the script is running.

Arguments

Color Value {RGB}.

A Red, Green, Blue color value in the format:

RGB(Red value, Green value, Blue value).

Other color values, such as hexadecimal color values can be used, but we recommend RGB values.

Returns

RGB

Example:

Mimic.BackColour = RGB(255,0,0)

This sets the background color of the Mimic to red (red value is 255, green and blue values are 0).

The Mimic.Backcolour property does not apply to embedded Mimics.


Disclaimer

Geo SCADA Expert 2022