Mimic.GoForward
            The Mimic.GoForward function allows the script to navigate from a Mimic to the next display. This only applies to Mimics that are in a 'chain'.
| Syntax | 
                             Mimic.GoForward()  | 
                    
| Description | 
                             Navigates from a Mimic forward to the next Mimic in the sequence.  | 
                    
| Arguments | 
                             None  | 
                    
| Returns | 
                             None  | 
                    
The script has no effect if the current Mimic is not part of a 'chain' of Mimics. The next Mimic can only be shown if there is a sequence (the sequence is created when hyperlinks to other Mimics are selected on a Mimic).
For an example, see Go to Next Mimic in Sequence.