ServerQuery.Error

The ServerQuery.Error property indicates whether the SQL Query for the Server.Query succeeded or failed.

Syntax

ServerQuery.Error

Description

Indicates whether the SQL Query for the Server.Query property has failed.

Arguments

None.

Returns

Error {Boolean}.

Returns a True value if the SQL Query for the Server.Query property failed or a False value if the SQL Query was successful (see Server.Query).

For an example that shows how the ServerQuery.Error property can be used, please refer to Server.Query.


Disclaimer

Geo SCADA Expert 2022