Slider.Minimum

The Slider.Minimum property is used to set the lowest value for the slider.

Syntax

Slider.Minimum = LowestValue

Description

Defines the lowest value on the slider.

Arguments

LowestValue {integer}.

Defines the lowest value that can be selected on the slider.

Returns

None.

Example:

Slider.Minimum = 10

This sets the slider range so that it begins at 10. There are no slider positions lower than 10.


Disclaimer

Geo SCADA Expert 2022