Using a Script to Access the Print Settings

You can use a script to display the print settings for a Mimic. When a user selects the relevant Mimic item, the Windows Print window is displayed. They can use the Print window to define the print settings and initiate a print-out of the Mimic.

The script for accessing the print settings is Mimic.Print.

Example:

Public Function PrintMimic

Mimic.Print

End Function


Disclaimer

Geo SCADA Expert 2022