Define the Operator Document Store for a User Group
You can associate each User Group with an Operator Document Store. The Operator Document Store that you choose will be available to the members of the User Group and can be used to store documents such as Trends (users that do not have the permissions to edit and save Trends will be able to edit and save the Trends in the Operator Document Store).
For more information on operator document stores, see Operator Document Stores in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
To define the Operator Document Store for a User Group:
- Display the User Group Form.
- Select the User Group tab.
- Use the browse button feature of the Operator Document Store field to select the operator document store for the User Group.
Operator Document Stores are special groups that can contain documents such as Trends. What is special about these groups is that they allow users that do not have the Configure permission to access the Edit and Save features for the items in the group. This means that operators can alter the configuration of a Trend to suit their needs and then save it in their Operator Document Store.
When you select an operator document store for the User Group, the members of the User Group will be able to edit and configure the documents in the selected store. Each user will also be able to edit and configure the documents that are in the store that is defined in the configuration of their individual user accounts.
- Save the configuration.
You can now associate user accounts with the User Group as required (see Associate a User with a User Group).