Hardware and Operating System Security

The security of Geo SCADA Expert is also dependent on the operating system as well as the hardware platform on which it is installed. The following sections are aimed at System Administrators who are setting up and configuring the systems prior to the installation of Geo SCADA Expert and are recommendations that should be considered to improve the general security. These aspects of the document are suggestions of good practice, but are not comprehensive, and need to be allied with recommendations for server and client configuration from the operating system software vendor, hardware vendor and security experts.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2022