Users List Headings

The Users List provides information about the users on your system.

Users List

The Users List can be filtered so that it only provides information about users with specific attributes.

When you display the Users List (see Display the Users List), you can view the following categories of information:

By right-clicking on any User in the list, you can access the context-sensitive menu for that specific User.

NOTE: The Password categories only apply to User Accounts that are managed directly in Geo SCADA Expert. With User Accounts that are associated with Windows or LDAP User Profiles, password management is performed via the relevant Windows domain or LDAP server.


Disclaimer

Geo SCADA Expert 2022