Communications Logging

Communications log files provide a record of communications between the drivers and the outstations and modems. They provide diagnostic information that can be used when investigating unexpected system activity.

There are 2 types of communications log file:

Advanced drivers support both types of communication log. Simple drivers have a hybrid type of log file that are a combination of IO and communications—these hybrid types of log file are also referred to as 'comms logs'.

If you contact Schneider Electric for assistance, you may be asked to create a communications log file.

There are separate log files for each channel. The names of the log files use the following format:

Driver<name> <port> <type>_<nnn>.log

Where:

For example, DriverSCADAPackModbus COM1 IO_001.log

To maximize system performance, you should only enable communications logging on a channel when required. You should leave communications logging disabled at other times.

This section includes:


Disclaimer

Geo SCADA Expert 2022