Define the Options for a List Field’s Drop-Down List

When you add an extra list field, you need to specify the options that will be available via the list field’s drop-down menu. To do this, you need to use the Categories settings on the Edit Field window.

List fields are often referred to as combo boxes or drop-down lists.

To access the Edit Field window, see Add or Modify an Extra Field. When you have displayed the Edit Field window, use the Categories setting to define the list options.

You can choose to:

When you have defined the Categories settings, you can continue to define the other field settings as required.


Disclaimer

Geo SCADA Expert 2022