Determine the Cause of the Failures

When you have displayed the port server's log file, you can use it to diagnose the cause of failures.

By default, the log file only records errors such as failures to assign to a serial port. Each error indicates:


Disclaimer

Geo SCADA Expert 2022