Dual Network Servers

Some servers are fitted with two network cards and so can support dual networking (multiple physical connections between network devices). Typically, dual network servers are used with Geo SCADA Expert to provide redundancy—they allow a server to have two physical connections to another server, meaning that should one network path fail, Geo SCADA Expert can use the ‘backup’ network path instead. Dual networking can also be used to isolate networks and to provide additional bandwidth.

To configure dual networking you can use Geo SCADA Expert's native network sharing feature, or the configuration features of the operating system and / or network card software. We recommend the latter, and to do this, you need to use Microsoft Windows Control Panel to configure Network Connections. In the configuration for each network card, you will need to define:

When you have set up each network card in Windows, you will need to configure Geo SCADA Expert to recognize the two network cards (see Configure the Main and Backup Connections).

Further Information

For more information on setting up network cards in Windows, please refer to the documentation supplied with your network cards as well referencing NIC Teaming for further advice.


Disclaimer

Geo SCADA Expert 2022