Manual Changeover

The manual changeover feature is for use on systems that have Hot-Standby Pair or Triple-Standby server arrangements. It allows you to define which server is the Main server.

There are many possible reasons for needing to perform a manual changeover. Two common uses are:

There are two ways to perform a manual changeover:

Further Information

System Architectures.

Check that Standby Servers are Synchronized with the Main Server.


Disclaimer

Geo SCADA Expert 2022