Miscellaneous Tab

You can use the Miscellaneous tab to configure the following settings for the server:

Main Server Deadlock Detection

The Main Server Deadlock Detection section allows you to enable and configure the monitoring of the database for the occurrence of a prolonged database deadlock event on the server currently acting as the MAIN.

You can use the Main Server Deadlock Detection feature in conjunction with, or independently of, the Database Watchdog feature. The latter feature can be used to detect whether the server has remained frozen for longer than a configurable amount of time, and if so, stop the server process and generate a minidump file that can be used to help analyze the cause (see Configure the Database Watchdog Settings).


Disclaimer

Geo SCADA Expert 2022