Parameters Settings (SQL Queries)
The SQL Query Configuration branch of the Server Configuration Tool includes a Parameters section.
You can use the properties in this section to define the SQL Query Parameters that apply when accessing the database from this particular Geo SCADA Expert server.
Use the settings to:
Further Information
The Edit Query option: see Ascertain which SQL Query is Presently used by a List.
Using SQL queries: see Welcome to the Geo SCADA Expert Guide to Working with SQL.
QueryPad (an SQL diagnostics tool): see Welcome to the Geo SCADA Expert Guide to QueryPad.