Remove a Severity Range
You can use the Geo SCADA Expert Server Configuration Tool to remove one or more severity ranges. If you remove the severity ranges, the default severities will be restored.
Whenever you remove a severity range, the alarms and events on your system are re-classified so that they correspond to the new range of severities.
ATTENTION: When you remove a severity range, the severity range that is immediately below the deleted severity in the hierarchy is increased. For example, if you are using the default severities, and you delete the Medium severity, the Low severity range will cover the internal values 1-666 instead of 1-333.
To remove a severity range:
- Access the Geo SCADA Expert Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool).
- Expand the Database Configuration branch of the tree structure.
- Select Severities to display the Severities section.
- Right-click on the Severity that you want to remove from the list of severities.
- Select the Remove option from the context sensitive menu.
The severity range is removed. - Right-click on the system icon in the tree-structure, and select the Apply Changes option to apply the changes.
Now that you have removed a severity, you can either proceed to configure other severities or you can continue with the server configuration.
If you are unfamiliar with the server configuration process, we recommend that you proceed to learn about Data Files Settings.