Remove an Extra Configuration Field or Extra Label

You can use the Metadata window to quickly remove those extra fields and labels that are no longer required:

  1. Display the Metadata Window.
  2. Select the Fields tab if you want to delete an extra field or select the Labels tab if you want to delete an extra label.
  3. Select the field or label that you want to remove.
  4. Select the Delete option.
    A prompt is displayed.
  5. Select Yes to confirm that you want to remove the extra field or label.
    The field is removed.

Disclaimer

Geo SCADA Expert 2022