Serial Connection Problems

If the port server fails to assign to a static serial port, the port server will log an error in its log file. You can use the log file to determine the cause of any problems relating to the port server. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

If the assign continues to fail, contact Schneider Electric for assistance.


Disclaimer

Geo SCADA Expert 2022