Understanding Geo SCADA Expert on Citrix and Remote Desktop Services

Geo SCADA Expert supports the two leading remote desktop applications: CitriX XenApp 5 and Microsoft Remote Desktop Services (formerly known as Microsoft Terminal Services). With remote desktop technology, the client applications run on a server and are not installed locally on the clients. However, each remote desktop client can access and interact with the server’s applications. This means that, to the end user, it appears as if the server’s applications are installed on the clients.

To make this possible, mouse movements, selections and keyboard entries on a client PC are sent to the server. At the server, the user interaction is applied to the actual application, and then graphics are sent back to the clients so that the user interfaces are updated.

When Geo SCADA Expert is used with remote desktop applications, Geo SCADA Expert is installed on the Citrix or Remote Desktop Services server. Each Citrix/Remote Desktop Services client can then access Geo SCADA Expert via ViewX or Virtual ViewX on the Citrix/Remote Desktop Services server. A separate instance of ViewX runs for each individual Citrix/Remote Desktop Services client, so to the end user, it appears as if they are using a ViewX or Virtual ViewX client.

A Geo SCADA Expert client configuration has to be configured for each Citrix/Remote Desktop Services client that is to access Geo SCADA Expert (see Citrix or Remote Desktop Services Client - System Connections).

The main purpose of running Geo SCADA Expert on a Citrix server or a Remote Desktop Services server is to centralize the ViewX application on a single server and allow clients to access ViewX or Virtual ViewX remotely. This reduces the overheads involved when upgrading and maintaining ViewX as the application is only installed on a single machine rather than multiple clients.

The following diagram shows a simple 1 Citrix/Remote Desktop Services server setup:

;

This simple setup involves a Geo SCADA Expert server which is connected to a Citrix/Remote Desktop Services server that is running ViewX (or Virtual ViewX). The Geo SCADA Expert server communicates with ViewX/Virtual ViewX on the Citrix/Remote Desktop Services server in the same way as it would communicate with any ViewX/Virtual ViewX client.

The Citrix/Remote Desktop Services server runs a single ViewX or Virtual ViewX application and is connected to the Geo SCADA Expert server and one or more Citrix/Remote Desktop Services clients. A separate ViewX session runs for each Citrix/Remote Desktop Services client, which allows the client users to interact with Geo SCADA Expert in the same way as if they were using a ViewX or Virtual ViewX client.

For each ViewX session, the Citrix/Remote Desktop Services server sends graphics to the clients (the graphics recreate the ViewX/Virtual ViewX interface on the client PCs). This allows the client PCs to provide access to the ViewX and Virtual ViewX interface. So the clients can be used in the same way as a ViewX or Virtual ViewX client even though they don’t have ViewX or Virtual ViewX installed locally.

Client user interactions, such as mouse clicks, selections and keyboard entries are reported to the Citrix/Remote Desktop Services server. There, the user interactions are applied to the corresponding session of ViewX/Virtual ViewX. The changes are then reported to the Geo SCADA Expert server where they are used to update the Geo SCADA Expert database and trigger actions on site, and so on.

Every time a client user logs on, a new session is created. The session associates an instance of ViewX or Virtual ViewX with that particular user, so that the user experience is just like working on a normal ViewX or Virtual ViewX client (even though the clients share a single ViewX or Virtual ViewX application). To make this possible, each session requires a Geo SCADA Expert license and a Citrix/Remote Desktop Services license.

More complex architectures work in the same way, except that there may be multiple Citrix/Remote Desktop Services servers (grouped into server ‘farms’). The key factors are that:


Disclaimer

Geo SCADA Expert 2022