Advise Threads

The Advise Threads category provides status information about the threads that are used to service the server advise links (the links from the server to a client).

There is an entry for each advise thread, and the entries are categorized as:

The number of threads varies according to the size of your system. For example, small systems may have 1 to 3 threads, whereas larger systems can have many more.

Typically, the Advise Threads information is used to detect possible connection problems (the number of threads can indicate this):

If you suspect that there is a connection issue, please contact Schneider Electric.


Disclaimer

Geo SCADA Expert 2022