Check for High Load on a Geo SCADA Expert server
You need to use the Server Links category to determine whether there is a high load on a Geo SCADA Expert server. You can then proceed to diagnose the cause of the high load, or check for client load or abnormal network conditions.
To check for a high load on the server:
- On the Geo SCADA Expert server, Run the Server Status Tool.
- Expand the hierarchy, then expand the Server branch, and select the Server Links category.
- The Server Links category provides status information about each link that is used by the clients to send data to the Geo SCADA Expert server (see Server Links).
- Use the Server Links information to determine if the cause is related to server loading:
- Examine the number of links. If the number is excessive in comparison with the number of clients that are connected to the server, there may be a server loading problem. However, the number of links is not the only indication of server loading problems (see next step).
- Examine the durations of the Longest Req entries. If the longest requests are 1000 ms or more, there may be a server loading problem. This is even more likely if there were an excessive number of links (see previous step).
- If you suspect there is a server loading problem, due to either or both of the problems indicated in the above procedure, proceed to Diagnose and Resolve the Server Load Problems.
- If there are no indications of a server loading problem, proceed to Attempt to Resolve Client Load and / or Network Problems.