Clients

The Clients category provides status information about each client on the server. The number of clients varies according to the size of your system.

Typically, the Clients category is used to check that clients have valid licenses (they will be unable to connect to the server if they have invalid licenses). It is also used to determine which clients have a connection to the server.

The status information for each client is categorized under these headings:


Disclaimer

Geo SCADA Expert 2022