Config Changes Searches

The Config Changes Searches category contains information about the searches that are currently requesting data from the Configuration Changes Auditing files. You can use the information to determine if a slow response to a Configuration Changes request is due to a large search or another factor such as abnormal network conditions.

The Config Changes Searches category displays the following information:

The ability to edit SQL queries that are used in query lists, including Alarm Summary Lists, can be restricted. This is done by restricting the availability of the Edit Query option on such lists. Access to this option can be restricted on either a per server, or per user, basis. When access to the Edit Query option is restricted, the restriction also extends to QueryPad, the SQL diagnostics tool that is supplied with Geo SCADA Expert. When the restriction is in place, users will be unable to connect QueryPad to the database. For more information, see Specify Whether SQL Queries can be Edited using the Clients on this Server, and see Define the SQL Editing Settings for a User.


Disclaimer

Geo SCADA Expert 2022