Define when the Server Status Tool is Updated

When you display the Server Status Tool, it contains the status data for the time at which the window was displayed. By default, the Server Status Tool is updated with the latest status data every second.

You can use the Server Status Tool menu to change the update setting so that the Server Status Tool is 'refreshed' with the latest data:

You can also use the Paused option to stop the Server Status Tool from being updated until the Paused option is deselected.

To define when the Server Status Tool is displayed:

  1. Display the Server Status Tool (see Run the Server Status Tool).
  2. Select the View menu, then select the required option:
    • Refresh Now—To update the status information immediately
    • 1 Second—To update the status information every second
    • 5 Seconds—To update the status information every 5 seconds
    • 10 Seconds—To update the status information every 10 seconds
    • 30 Seconds—To update the status information every 30 seconds.

Disclaimer

Geo SCADA Expert 2022