Queued System Calls
The Queued System Calls category provides status information about the system calls that are waiting to be executed (they have been triggered to be executed, but cannot be executed immediately as other system calls are still in progress).
Each entry in the Queued System Calls category represents one system call i.e. one system command that is waiting to be executed by Geo SCADA Expert.
The status information is categorized as:
- Id—The number that Geo SCADA Expert uses to identify the system call reference.
- Command—The command that is performed when the system call is executed. This matches the command that is entered in the configuration of the corresponding System Call database item.
- Time—The time at which the execute command was triggered for the system call.
- Waiting—The amount of time the system call has been in the queue i.e. waiting to be executed.