Configure the MPI Station Parameters

When the Connection Type is set to MPI via serial adapter, use these fields on the Connection tab(s) to configure the Station Parameters:



Disclaimer

Geo SCADA Expert 2022