Point Count
Associated with: Sofrel outstations
The Point Counts indicates how many points of each type that the outstation has configured (SOFBUS-PL protocol only).
DI <n>, AI <n>, CI <n>, DO <n>, AO <n>
where <n> is the number of points in the outstation, ((see Source) for additional details of point types).