Upload Configuration and Parameters

Associated with: Sofrel S500 Series Outstations.

Security permission required to access this pick action: Configure.

The Upload Configuration and Parameters action is available for Sofrel S500 series outstations using the LACBUS-RTU protocol. These outstations are pre-configured before being connected and setup within Geo SCADA Expert. You can use the Upload Configuration and Parameters action to upload the configuration and operating parameters of points from the outstation when you have configured the following Sofrel items:

When you select the Upload Configuration and Parameters action the configuration for each point that exists within the outstation is created within Geo SCADA Expert, within the same group as the outstation. If the points already exist in the database they are just updated.

Call recipients that are configured in the outstation are also be uploaded, however this doesn't include Master Station and Remote Terminal Unit recipients as these cannot be uploaded. (see Sofrel Call Recipients).

The following settings are uploaded for each point:

This action is only available if the protocol for the outstation is set to LACBUS-RTU.

If the upload includes the configuration of points that do not exist in Geo SCADA Expert, Geo SCADA Expert creates the appropriate points automatically in the same group as the outstation item. If the point already exists in the Geo SCADA Expert database, Geo SCADA Expert just updates the configuration settings to match those of the upload.

NOTICE

LOSS OF CONFIGURATION CHANGES

When you upload the configuration from an outstation it will overwrite any existing configuration for the outstation in Geo SCADA Expert. For this reason, take care as you may lose configuration settings you have applied in Geo SCADA Expert.
Always verify that the configuration you are uploading is the correct configuration for the Outstation.
Failure to follow these instructions can result in loss of configuration changes.

Uploading to Group Instances

If you are going to upload the configuration, and the Outstation or any of its points are in a Group Instance, you need to be aware of:

If you upload configuration into items in a Group Instance (the Outstation or any of its points), Geo SCADA Expert has to determine which configuration to use. It compares the uploaded configuration settings to those that are already in place in the Geo SCADA Expert database, on a field-by-field basis. If the upload configuration settings are different to those in Geo SCADA Expert , Geo SCADA Expert checks if the required Property Overrides are defined. If they are, the upload configuration overwrites the existing configuration. Any settings that are the same as those in Geo SCADA Expert are discarded. If the upload contains points that do not exist in Geo SCADA Expert, new items are created to store the configuration. These new items are created automatically.

If an upload fails as a result of missing Property Overrides or point conversions being required, Geo SCADA Expert lists the configuration errors in a configuration report (see Configuration Reports for Sofrel Outstations). There are no changes made to the Geo SCADA Expert database.


Disclaimer

Geo SCADA Expert 2022